STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to connect VREF+ pin on stm32F722RET6?

I am designing a custom PCB using STM32F722RET6. How to connect the VREF+ pin(13) on the SMT32F722RET6?.As per the hardware development manual, it says"The VREF+ pin can be connected to the VDDA external power supply"and then, "VDDA=VDD and VSSA=VSS...

VKoga.1 by Associate II
  • 1880 Views
  • 2 replies
  • 0 kudos

Resolved! In NUCLEO-L432KC Is it possible to use pins PB6 and PB7 if I have allocated pins PA9 and PA10 for the I2C1 port?

Hi ST community,I'm working with NUCLEO L432KC and in my application I need to use I2C1 port. Using STM32CubeMX to generate the project, I could see that when I enable the I2C1 port, Automatically the CubeMX allocate the PA9 and P10 pins. For my appl...

VNava.1 by Associate III
  • 3542 Views
  • 1 replies
  • 0 kudos

Resolved! Don't drive LEDs from these pins. "PC13, PC14 and PC15 are supplied through the power switch". What does this power switch really do?

SummaryAt the end of the day, my issue is missing something in documentation. The lesson here, is test thoroughly. Just because it works for a few minutes, doesn't mean forever. Anyway, I've been running >3mA through the pins that are limited before ...

0693W00000DmnGQQAZ.jpg 0693W00000DmnaVQAR.jpg
DJC by Senior
  • 2953 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L011F3U6TR mcu boot0/PB9 pin has internal pull-up/pull-down resistor feature?

Please help to find out whether STM32L011F3U6TR mcu boot0/PB9 pin has internal pull-up/pull-down resistor feature. There is no mention that boot0 pin is special in this respect, ie no internal pull-up/pull-down resistor.  On my board, unable to bring...

STlink V3 connections.

I want to be sure of the interconnects between the STlink and STM32 that will give me full debug capability using the CUBEIDE development environment. It would require 4 connections; 3.3v,gnd, SCLK(PA13) and SDIO(PA14). Some STM docs identify two add...

CSopk.1 by Associate II
  • 5901 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.