2024-12-15 10:46 PM - last edited on 2024-12-15 11:55 PM by mƎALLEm
Hi,
I am having STM32U575ZI-Q development board. I have implemented a firmware with FreeRTOS with low power support where the firmware goes to the low power mode and unless there is an external interrupt, it stays in a low power mode.
Now, I want to measure the current ocnsumption when the MCU goes to the sleep mode (STOP2 mode specifically). Is there anyway I can measure the current from the STM32Cube IDE or any addtional board that can be interfaced with the development board?
Solved! Go to Solution.
2024-12-16 1:26 AM
Hi @mdalal !
Not possible for you to measure the current from the MCU through jumper JP5 with a DMM?
JP5
2024-12-16 1:26 AM
Hi @mdalal !
Not possible for you to measure the current from the MCU through jumper JP5 with a DMM?
JP5
2024-12-16 2:02 AM
Oh, do you mean that if I connect the DMM across this jumper pins, the job is done? What precision of DMM is required.
2024-12-16 2:11 AM
I am assuming that the DMM is in current measurement mode.
2024-12-16 2:26 AM - edited 2024-12-16 2:29 AM
@mdalal wrote:I am assuming that the DMM is in current measurement mode.
Yes, of course.
@mdalal wrote:Oh, do you mean that if I connect the DMM across this jumper pins, the job is done? What precision of DMM is required.
Yes. The precision of the DMM depends on your requirements. Personally I would prefer a DMM with you can at least measure 1µA.
The possible power consumption from the MCU in different situations are also described in the device datasheet. Here is a screenshot:
2024-12-16 2:41 AM
Great. I will try to get such DMM within and will let you know. You can close the ticket meanwhile.
2024-12-19 5:41 AM
Hello,
>> You can close the ticket meanwhile.
You can do that by clicking on the "Accept as Solution" button in the answer that helped you the most.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.