2026-02-11 8:14 AM
Hello everyone,
I recently bought the NUCLEO-N657X0-Q and I am trying to debug it using the ST-LINK_gdbserver.
Also this is my first development board and I don't know where to look. The data sheet and reference manual give me nothing in this regard and I am helpless.
Here is the command line output:
$ /opt/ST/STM32CubeCLT_1.20.0/STLink-gdb-server/bin/ST-LINK_gdbserver --swd \
-cp /opt/ST/STM32CubeCLT_1.20.0/STM32CubeProgrammer/bin -v -l 31 --frequency 8000 -k
STMicroelectronics ST-LINK GDB server. Version 7.12.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
InitWhile : Enabled
COM frequency = 8000 kHz
Target connection mode: Under reset
Target not halted after reset. Force halt
Failed to halt target
Target not halted
Error in initializing ST-LINK device.
Reason: Target not halted.I am on macOS Tahoe 26.2.
I have ruled out that it is due to connectivity problems because I can program the board and run software on it using the STM32CubeProgrammer and its corresponding STM32_Programmer_CLI. I can also halt the core, inspect memory, read system registers and configure peripherals. I have also not encountered anyone with a similar problem on the internet. BOOT0 is LOW and BOOT1 is HIGH to enter development boot. The board is connected through the CN10 USB-C port and the 5V_PWR LED (LD1) is ON. Also the PWR status tricolor LED (LD4) is GREEN which indicates that the power delivery is okay.
I got a simple blinking LED to work with basic GPIO but more complex projects require a debugger. I am deliberately avoiding the STM32CubeIDE because I do not want any hardware abstractions, but even CLion throws this exact error when I try to connect.
Please help me resolve this issue, I would be grateful!
For certainty here are more details from the STM32_Programmer_CLI:
ST-LINK SN : 003C00184142501420353451
ST-LINK FW : V3J16M8
Board : NUCLEO-N657X0-Q
Voltage : 3.28V
SWD freq : 8000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x486
Revision ID : Rev B
Device name : ST32N657
Device type : MCU
Device CPU : Cortex-M55
BL Version : --
Thank you in advance!
2026-02-12 5:14 AM
Hello,
I don't know about GDB server nor MacOS, but with GDB you have :
>> Target connection mode: Under reset
and with STM32CubeProgrammer_CLI, where it works:
>> Connect mode: Normal
>> Reset mode : Software reset
So based on the GDB server User Manual I would at least try to remove the -k option.
-v -l 31 --frequency 8000 -k
I don't know much more...
>> STM32CubeIDE because I do not want any hardware abstractions
You don't have to compile/call the HAL/LL libraries when you're using the CubeIDE, you can make direct register accesses as well, if that's what you mean.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.