Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I installed stsw-link009 on my pc so I could use the STLinkv3. The PC did not see the STLink-v3. I then installed STM32Cubeprogrammer thinking that would fix the stlink driver issue but when I look under devices USB in the device manager I can not se...
Respected ST Team, We are planning to purchase the STM32H7B3I-EVAL evaluation board and would like to confirm the accessories included in the standard package before placing the order. Order link is https://www.st.com/en/evaluation-tools/stm32h7b3i-e...
Hi everyone, I'm designing a board with an STM32H7[STM32H757XI] and two MT48LC16M8A2P SDRAM chips to get 16MB (16-bit wide). I'd appreciate a schematic review before PCB fabrication. Hardware:- MCU: STM32H757XI- SDRAM: 2x Micron MT48LC16M8A2P (4Mx8, ...
i have been trying to find ways of converting my stm32f103 board to stlink for a personal project , i have found out i need to flash the st link firmware onto this chip but i am not really able to understand how to flash this on the board , if someo...
I am designing a 4 layer PCB which uses an STM32L433 and working on the layout for the LSE and HSE crystals. I referred to the application note AN2867 for guidance, but I am confused by the isolated ground plane underneath the crystals as shown in F...
I have been using PE micro Multilink FX for several years, but its Linux support is terrible. Is there a ST (or another) alternative with this functionality compatible with stm32CubeIDE? I just need to supply power (up to 100 mA at 3.3V) to my board ...
Hello everyone, I recently bought the NUCLEO-N657X0-Q and I am trying to debug it using the ST-LINK_gdbserver.Also this is my first development board and I don't know where to look. The data sheet and reference manual give me nothing in this regard ...
Are the design files of this board available from ST website? I'd need to know where can I get 3.3V and tie it to pin1 (Target VCC) off CN14. Then I'll be able to power the target MCU through this connector. Please check next post for further informa...
I am configuring the RTC and using the user button on NUCLEO-H563ZI, but it is not working as expected. When I check the configuration in .ioc, I see that yellow signal in the RTC section. I have checked it and do not understand what is happening.Cou...
Hi, I am facing an issue while connecting to my board using STM32CubeProgrammer and ST-LINK. I would appreciate any help. Board: NUCLEO-F072RBProgrammer: ST-LINK (Onboard)Software: STM32CubeProgrammerConnection: SWDST-LINK Firmware: V2J46M31 Issue De...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.