2024-09-02 9:49 AM - last edited on 2024-09-06 9:42 AM by mƎALLEm
Im using NUCLEO-H755ZI-Q. I used it together with plattformio and arduino framework. In order to get arduino to work im using this setup:
[env:nucleo_h743zi]
platform = ststm32
board = nucleo_h743zi
framework = arduino
monitor_speed = 115200
Error: init mode failed (unable to connect to the target)
As well as the board is not connected stm32CubeProgrammer.
Solved! Go to Solution.
2024-09-06 1:15 PM - edited 2024-09-06 1:17 PM
Yes NUCLEO-H745ZI-Q but dioesnt support arduino framework. What aboutwhat about something like Nucleo-F767ZI or NUCLEO-H753ZI? Are these both fully supporting arduino framework? Then maybe that would be an alternative. My criteria is the fastest board possible with about 100 gpio
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.