2024-09-05 2:19 PM
Hello ST Community,
I am connecting you because I am trying to use a Waveshare LCD/TFT screen (https://www.waveshare.com/2.8inch-tft-touch-shield.htm) which uses the ST7789 (lcd) and XPT2046 (TFT) chips. I can make it work with an Arduino Leonardo board. However, I cannot implement it with the NUCLEO-F401RE board. More precisely, I can implement the backlight (by driving a GPIO), but the SPI communication does not seem to be working. Would you be able to confirm that pins PA5 should be used for SCLK, PA6 for MISO, PA7 for MOSI and PB4 to PB6 for: SD_CS, TP_CS and LCD_CS ?
There are several git repo with different code drivers version, but not sure about SPI1 pinout.
Do you have a link to a driver that can be used with the NUCLEO-F401RE board or any advices for debugging ?
Thank you very much for any help you can give me.
Best regards,
Solved! Go to Solution.
2024-09-05 2:49 PM
The ZIP with the source codes from Waveshare also contains the ioc files of the projects for STM32, which are based on STM32F103 but can be converted to STM32F401.
PA5 is already assigned to LD2 on the NUCLEO, but you can easily change this by opening SB21, for example, and thus disconnecting LD2. If you then set pin PA5 to Reset_State again with STM32CubeMX or STM32CubeIDE, you can easily set SPI1 to full-fuplex master and thus assign MOSI, MISO and SCK.
2024-09-05 2:37 PM
The pin assignments should be derived from the NUCLEO-F401RE User Manual, or Schematic under the CAD Resources tab on the product page.
https://www.st.com/en/evaluation-tools/nucleo-f401re.html
D13 PA5 SCLK
D12 PA6 MISO
D11 PA7 MOSI
D10 PB6 LCD_CS
D9 PC7 LCD_BL
D5 PB4 SD_CS
D4 PB5 TP_CS
Should be several drivers you could port to the platform
Use the SPI TransmitReceive function to get good timing with respect of GPIO for CS going LOW/HIGH
2024-09-05 2:49 PM
The ZIP with the source codes from Waveshare also contains the ioc files of the projects for STM32, which are based on STM32F103 but can be converted to STM32F401.
PA5 is already assigned to LD2 on the NUCLEO, but you can easily change this by opening SB21, for example, and thus disconnecting LD2. If you then set pin PA5 to Reset_State again with STM32CubeMX or STM32CubeIDE, you can easily set SPI1 to full-fuplex master and thus assign MOSI, MISO and SCK.
2024-09-06 11:26 AM
Thank you Peter and Tesla De Lorean for your support. Your proposals help me to fix the issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.