2020-12-07 4:24 PM
Basically I got the tool chain working on Linux Mint 20.0 with the STM32 CubeIDE v1.5.0, downloaded and installed today.
My device is a Blue Pill (genuine STM32F103C8T6).
It's connected with an STlink v2 via SWD (Firmware version V2J37S7).
Boot0 and Boot1 are both high via a 100k resistor to 3V3. I can program the device with PlatformIO, but not with the CubeIDE from STM. The Error Message:
Error in final launch sequence:
Failed to start GDB server
Failed to start GDB server
Error in initializing ST-LINK device.
Reason: (4) No device found on target.The Console output:
STMicroelectronics ST-LINK GDB server. Version 5.7.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.Currently I have 2 workarounds:
STMicroelectronics ST-LINK GDB server. Version 5.7.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.6.0-RC3
-------------------------------------------------------------------
ST-LINK SN : 36FF6A064D59303621422343
ST-LINK FW : V2J37S7
Board : --
Voltage : 3,24V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x410
Revision ID : Rev X
Device name : STM32F101/F102/F103 Medium-density
Flash size : 64 KBytes
Device type : MCU
Device CPU : Cortex-M3
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_EKblf8.srec
File : ST-LINK_GDB_server_EKblf8.srec
Size : 8756 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 8]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.613
Verifying ...
Download verified successfully
Error in executing 'detach' command ...
Debugger connection lost.
Shutting down...
2020-12-07 5:40 PM
> set Boot0 pin to 3V3 (via 100k resistor) again, press reset, now the new program is running
Are you sure? Setting BOOT0 high during will run the built-in bootloader, not your program.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.