STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GPIO Pin not going High

I'm using a Nucleo-H723VG board and trying to use the PB8 and PB9 pins. I'm able to set PB9 high and see a voltage of 3V but for PB8 it only shows a voltage of 359mv. I have tried enabling the internal pullup and still doesn't go high to 3V.The yello...

jasd33p_0-1725464875313.png
jasd33p by Associate II
  • 3791 Views
  • 9 replies
  • 4 kudos

Resolved! I2C clock incorrect

Im using the stm32f407 discovery to run I2C in fastmode (400kHz), using the equation given in the datasheet, I choose the system clock to be 120Mhz, so I have 30Mhz pclk for I2C. duty cycle T_low/T_high = 2, so CCR is 25d, T_rise is 300ns so that wou...

Screenshot (91).png
NoNamed by Associate II
  • 2188 Views
  • 3 replies
  • 1 kudos

Resolved! NUCLEO-F767ZI Ethernet Problem

Hi Team, I am Using NUCLEO-F767ZI board for Ethernet interface. After all Ethernet configuration. The code shows lots of error which is attached below. Guide me how to rectify this error, what mistake I was done during configuration and programming.T...

Ramachandran1992_0-1722408760388.png Ramachandran1992_1-1722408950710.png

Resolved! NUCLEOF767ZI Ethernet LWIP problem

Hello, I'm new to STM32CubeIDE so I need you not to go too hard with explanations :).  In these weeks I'm working on a project that uses ethernet based on the NUCLEO F767ZI board using the LWIP library.After consulting the PDFs available on the F767Z...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.