STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-LINK Server for ARM Linux Platform

Posted on May 28, 2018 at 22:41Special request:Could the ST development team please compile the http://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-performance-and-debugger...

STM32 ST-LINK Utility Programming error

Posted on May 17, 2018 at 14:24Hi everyone,I have a very strange behavior using the STM32 ST-LINK Utility v4.2.0.0. While flashing a specific HEX file, the error message 'Programming error @ 0x08008C00' is occuring.When I use the uVision Keil Flash ...

ame by Associate II
  • 3687 Views
  • 2 replies
  • 0 kudos

How to use ST-Link Server?

Posted on April 09, 2018 at 08:16Hi all,I installed the ST-Link Server and after starting it, it opens up the default port 7184 on the local machine. But I have no idea how to interact with it. It's not a HTTP server, because using it over a browser...

Josh Yu by Associate II
  • 1723 Views
  • 2 replies
  • 1 kudos

Nucleo-F070RB and ST-LINK/V2

Posted on May 04, 2018 at 10:22It seems that in my Nucleo board the embedded debug interface (the USB) is broken. How do I connect an external ST-LINK/v2 to the board to be able to flash SW and debug? The debugger should also power the board.#st-lin...

ST Link Communication Error on STM32F411

Posted on April 25, 2018 at 15:10I have an STM32F411 on a PCB and I tried to connect it to the ST link using STM32 ST-Link Utility app but I get the error Cannot connect to target! Please select 'Connect Under Reset' mode from Target->Settings menu....

STM32F746 Discovery pcb project

Posted on April 16, 2018 at 16:47I need the pcb project for STM32F746 Discovery. I have the schematics, BOM, gerbers but the pcb project. Can I find it somewhere?Thanks,Denin#pcb-project #stm32f746-discovery

Den In by Associate II
  • 2726 Views
  • 6 replies
  • 0 kudos

ST-Link and reading 0xC0000000

Posted on April 16, 2018 at 13:36I have a ST32H7 project on the go with SDRAM at 0xC0000000. I can read internal memories via ST-Link and SWD just fine in a live system and this is helpful during debugging. However, try to read the initialized and w...

info by Associate II
  • 2843 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.