STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Fluctuation in the high voltage level

Posted on June 26, 2018 at 09:00In STM32F411 Discovery board, The STlink was not able to program the on board STM32f411, so i have usedSTLink /v2 external module to load the program into MCU. I have also applied the target voltage 3.3V to the board ...

Is it mandatory to cut off the Nucleo board in order to use PA13 and PA14 to program with ST-Link/v2?

Posted on June 25, 2018 at 18:59Hi everyone,I play with a Nucleo-F767ZI, using the ST-Link part provided on the PCB.I would like to use a ST-Link/v2 to program my MCU.I was wondering, whether it is possible to power my MCU (without USB PWR) and use ...

0690X0000060BrtQAE.png 0690X0000060BnnQAE.png
ced seg by Associate II
  • 2033 Views
  • 2 replies
  • 0 kudos

ST-Link v2 Upgrade Error

Posted on June 10, 2018 at 16:13Hi, I'we got a ST-Link v2 USB dongle.The firmware on it is:  V2.J17.S4Trying to upgrade the firmware to the latest V2.J30.S7I'm using the software provided by ST: ST-LinkUpgrade_007(both win subfolder and java)STM32 ...

ST-Link V2 corrupt

Posted on June 02, 2017 at 02:14Hi,Today I noticed that the ST-Link on STM32F0Discovery board lost the connection with the MCU after about 10 seconds. I tried another programmer and that worked perfectly so something wrong with the Discovery board. ...

0690X00000607CrQAI.png
anagy9 by Associate II
  • 3152 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.