2018-05-06 6:30 PM
Hi
I've been using STM32F407VG for a long time. Today i got an error when i plug in my laptop and i can not solve this problem over 8 hours. When i connected the STM to PC, the error message was USB Device Not Recognized - Error Code 43. We tried a lot of ways to fix the error such as STM, enter device manager uninstalled and reinstalled. While i pressed the reset button, i tried to load the code on Keil v5, but the two error messages were no ST-LINK detected (Debugger - Cortex-M error) and flash download failed target dll has been cancelled. I have tried to do it on the board some SWD pins, i tried to do cirtcuit close with jumpers
#st-link-detected-administrator #usbSolved! Go to Solution.
2018-05-09 11:00 AM
Hi,
The issue not about software, it's about hardware. I measured between +5V - GND. The value of voltage was 2.5V
I realised that i had short circuit between +5V and GND. So D1 diode has been broken down. Then i removed D1 and replaced by Diode D2. Then I measured between +5V - GND again. The value of voltage betweeen +5V - GND is now 5V. So STM32F4 works properly.
2018-05-08 7:32 AM
Hi
fvarlii
,Use
or and try to make a Firmware upgrade of the STLink, then gain after that.-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-05-09 11:00 AM
Hi,
The issue not about software, it's about hardware. I measured between +5V - GND. The value of voltage was 2.5V
I realised that i had short circuit between +5V and GND. So D1 diode has been broken down. Then i removed D1 and replaced by Diode D2. Then I measured between +5V - GND again. The value of voltage betweeen +5V - GND is now 5V. So STM32F4 works properly.
2018-05-09 11:00 AM
Thank you for attention
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.