STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Greyed interface in ST-Link Utility

Posted on April 11, 2018 at 17:05Hello everyone, I am having issues with ST-Link utility. Whenever I first launch it, everything looks fine, but if I try to change something in the settings (such as 'connect under reset') and then I press OK, the se...

B C by Associate II
  • 5033 Views
  • 12 replies
  • 0 kudos

[STM32] No voltage on VDD_TARGET pin

Posted on April 12, 2018 at 23:51I have a microcontroller (STMF103RET) mounted to the adapter. I would like to program it using the ST-Linkv2 programmer from the Nucleo board (STM32F103RB). According to the instructions, I disconnected the CN2 jumpe...

0690X00000604ZiQAI.jpg 0690X00000604ZnQAI.jpg
bastik * by Associate
  • 1850 Views
  • 1 replies
  • 0 kudos

if i have st-link v2 then do i still require any usb interface with STM32F4 for firmware upgrade or program update?

Posted on March 30, 2018 at 10:14I'm going to develop stm32f4 board for my application but i have no more space so i'm thinking the use of ST-Link V2 utility for program the processor and upgrade the firmware. so is it possible with ST-link v2 utili...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.