Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello everybody,I am developing an embedded application using STM32L562E-DK which autonomy has to be greater than 3 months.My problem is that I remarked that the board consumption (not including the MCU and its peripherals) is about 120 mA. I precise...
I have an ST-LINK / V2 Programmer with the number B 2018 33 containing Firmware V2.J27.S6, we are completely satisfied with it. The service needs in the field forced us to buy another ST-LINK / V2 with the number A2021 03 containing Firmware V2.28.S7...
I have custom board based on G431CBT6 which's based on B-G431B-ESC design without any issues, however I need more pins such as more UARTs and ADCs therefore I made another custom board which's based on G431RB 64 pins, how the problem is the SysTick_...
I have a STM32H735-DK and I'm trying to load the LedToggling sample app with the STM32CubeIDE 1.5.1. Debug fails with this message.Starting server with the following options: Persistent Mode : Disabled LogFile Name ...
I have a board (MCU: STM32H7B3LIH6Q) that I've been trying unsuccessfully to connect to using an external J-Link module, and recently I've switched to the internal ST-Link debugger. However, when I try to connect on STM32CubeProg for software reset, ...
Hello, I just wanted to ask if I bought the NUCLEO-L4R5ZI-P devlopment kit before implementing the STM32L4S5ZI into my PCB. Will it still work with the same code?Thank you Hanya
I've been working with the STM32H7B3LIH6Q board on Segger, and it was functioning normally until I happened to flash the code below to it. Now I get "no idcode detected" on Segger and "No debug probe detected" on STM32CubeProgrammer when connected to...
Hello dear engineers,I have made a custom header board based on the STM32f429BIT6. The board can be programmed with the JTAG interface. AS SWD and JTAG share the same connection, (JTAG needs more connection), I assumed that it would be possible to ch...
Hi, I'm trying to design the USB OTG function on my PCB with STM32L4R5ZI. I saw the training documents and video on ST website and I'm confused about how to connect the TVS diode. There's a youtube video as well. Since I'm using the OTG function, it...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.