Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
The Nucleo we are using has build in ethernet module.
Dev board: Nucleo-F767ZIDear all,as I wanted to have my own Vref+ for ADC conversions I removed solder bridge SB12 (coupling Vref+ with VDD) to input my own reference voltage (~3V) at Pin 6 CN7.After removing the SB12 however the STM 32 device is not...
I'm having trouble updating the firmware of a X-NUCLEO-BNRG2A1 using the procedure described in AN5651 page 4 ("Direct update on the X-NUCLEO-BNRG2A1 expansion board" through the NUCLEO64-L476RG integrated ST-LINK 2-1).I get this error message in FAI...
Hi,I connected my brand new STM32F769I EVAL board to power and to PC through USB ST-Link port, I opened STM32CubeProgrammer, picked ST-LINK connection on the top right, clicked Connect, and it said that I need to perform a firmware update first. So I...
I am using the ST-Link CLI tool in windows.I am able to progam a virgin unit and after a power cycle the correct software is runningHowever a need to make a testjig setup. The unit is powered by USB so after programming I need to reset the unit to ru...
Dear All,I am designing a card using STM32F730R8 whose package is LQFP64. Datasheet makes me confused. Let me explain step by step.1- Datasheet Page 50: There is a pinout figure and it shows that Pin 13 is VDDA.2- Datasheet Page 57: There is a table ...
We are using STM32H750IBT6 Micro in our project and i'm trying to read external flash which is QUADSPI Flash (MT25QL128A) by ST-Link V2 using STM32 Utility/Programmer. I am able to read and write microcontroller but unable to read and write external ...
I am using KIEL with ST-LINK V2 programmer Boot0 ( Pin number 138) tied to LOW via 10K resistornRST has a 100nF to GND and a pull up resistor 10KChecked the POR and it looks fine It looks like the chip doesnt run Please advise
STM32 STLINK Utility has stopped working. I'm sending the setting. What could be the reason?[Settings] File= address=0x08000000 size=0x1000 data_width=4 connection=SWD SwclkFrequency=15K freq=8000 Connection_Mode=Normal DebugInSleepMode=1 Reset_Mode=...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.