2021-06-23 9:39 AM
I have custom board based on G431CBT6 which's based on B-G431B-ESC design without any issues, however I need more pins such as more UARTs and ADCs therefore I made another custom board which's based on G431RB 64 pins, how the problem is the SysTick_Handler routine in stm32g4xx_mc_it.c has never called, can anyone know what's different between CB and RB ?
danny
2021-06-23 11:24 AM
> can anyone know what's different between CB and RB ?
The package and related things (number of pins, footprint) are different, that's it.
2021-06-24 5:45 AM
i understand that, for CB scale up to RB all of the pins are same, and I also check the STM32G431RBTX_FLASH.ld and startup_stm32g431rbtx.s files but found no different.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.