STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L431 DAC

Which DAC method is used for STM32L431, R-2R or resistor strings?Different things are written in the two materials. https://www.st.com/content/ccc/resource/training/technical/product_training/01/4b/81/0e/21/a6/4c/55/STM32L4_Analog_DAC.pdf/files/STM32...

kazuchib by Associate II
  • 4164 Views
  • 6 replies
  • 0 kudos

Resolved! HW design

Hello, I have to design a circuit and I need help. There are two external devices, which the third device with MCU STM32F105 has to find out which of them is connected to it. Two external devices have signals:- 24v or non-connected - GroundI can mayb...

NASI by Senior
  • 3079 Views
  • 6 replies
  • 0 kudos

Hi I got an ST Link ISOL for programming an STM32L4R9 on custom board. I can connect it to ST Link V2 on SWD using 4 pins from another nucleo board, TGT_VDD, SWCLK, SWDIO and GND.

In the target voltage I can see not detected. I have removed the ribbon cable and have connected using jumpers now, pins in the following manner:1 - VDD7 - SWDIO9 - SWCLK3, 6 - GNDI don't know what is going wrong with the ISOL version of the STLINK v...

Makarand by Associate II
  • 2960 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.