2022-02-16 1:24 AM
Hello,
I'm using the X-NUCLEO-LPM01A Board. Today I encountered a problem with the calibration. If I set the voltage to 3.3V and run a calibration I measure at VOUT only 3V. Without any calibration I measure the expected 3.3V. If I set the voltage to 1.8V and run a calibration I measure also 3V at VOUT. Without calibration it's 1.8V. Have you seen this problem? Or do I something wrong? Maybe I have to set the voltage after calibration again?
Solved! Go to Solution.
2022-02-16 11:54 PM
This issue has been fixed in the new firmware version [v1.0.7] of STM32-LPM01-XN.
Here is the link to access the last one of the firmware:
2022-02-16 11:54 PM
This issue has been fixed in the new firmware version [v1.0.7] of STM32-LPM01-XN.
Here is the link to access the last one of the firmware:
2022-02-16 11:56 PM
Great!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.