cancel
Showing results for 
Search instead for 
Did you mean: 

Se puede alimentar STM32F103C8T6 por USB a través del ST-LINK V2, mientras el Hardware (SENSOR) está alimentado con una fuente externa? La idea es visualizar mediciones del ADC1 con CubeMonitor desde la PC.

FGRAMOY
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @FGRAMOY​, to the community!

I've translated your question with a web-based translation tool to increase the chances that you will get an answer from our experts and community members, as the majority communicate in English:

Can STM32F103C8T6 be powered by USB via ST-LINK V2, while the hardware (SENSOR) is powered by an external power supply? The idea is to visualise measurements of the ADC1 with CubeMonitor from the PC.

You have not specified your hardware configuration because this depends on various factors:

  • Are you using an original ST-LINK/V2 from ST?
  • Do you have your own hardware with STM32F103 or a development board like NUCLEO, DISCOVERY or EVAL?
  • What is your sensor connected to?
  • What voltages does your sensor output?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.