Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
HelloI have encountered a strange problem at work using stm32f439zi processors.Some context:We're using two board:development board NUCLEO-F439ZI, with a processor stm32f439ZITx in revision 4custom board, with a processor stm32f439ZIYx in revision 3T...
Hello!For some weeks, I have been using an STM32F769I-DISCO board as the centrepiece of a new industrial solution which enables us to know how much paper has been consumed by a studied machine. Therefore, firstly, an inductive sensor is used and gene...
I'm working on a board design with a STM32F103C8. First time for me to build a PCB with STM32, I've always worked with "blue pill" boards.Not sure about BOOT wiring. The firmware will be uploaded using STM32CubeProgrammer. The board should startup us...
Posted on March 10, 2018 at 12:57I am trying to program my STM32F103C8T6 from ST link utility but it is showing 'Some Flash Pages are write protected'error while performing full chip erase. I have tried direct programming option in st link utility b...
I use the STLINK-V3MINI in combination with STM32CubeIDE and STM32G4x µC. With SWV a tracing of 2 variables with 20kHz is possible without data loss. What are the limitations of the STLINK-V3MINI, and what justifies the purchase of an expensive debug...
Hello,I want to build a small Python application that reads out data from my STM32 via ST-Link and SWD. Unfortunatelly I could find only one Python project providing something like this: PySWD. This one uses PyUSB and this one does not detect may ST-...
By default the ST-Link Debugger setting Pack "Keil.STM32L0xx_DFP.2.1.0" is Enable and I got error "Invalid ROM Table" when trying to flash the MCU. But If I just Disable the checkbox Enable in the Pack tab in ST-link Debugger setting then the flashi...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.