Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I am working with the NUCLEO-L552ZE-Q and have made a very simple test circuit to test an open drain output signal. I have the pin configured as an open drain output with no pull up or pull down with the signal pulled up to 3.3V through a 1K resistor...
The revision history of the manual says that the schematic was removed in late 2021. Where I can download the "removed" documentation file? What was the purpose of removal?
I'm making a PCB for a project and am using the STM32F411CE (Otherwise known as the "Black Pill"). However, after spending many hours looking through the data sheet and searching online I'm still not 100% sure I understand how to power this board via...
Hi,I tried to run OpenOCD on a virtual machine with Windows Server 2016. We using the version 1.3.0 of the STM32CubeIDE. When I launch the OpenOCD the program crahses with the error message: OpenOCD is launched via this command:CALL %PATH_STLink-OPEN...
i want to make PLC using STM32.in PLC circuit there is no STLINK programmer still we can program and debug(simulation) PLC How can i do this?below delta PLC images. There is no separate debugger or programmer in pcb.
Hello,We have CI/CD pipeline running in a build server with an ST-LINK attached to program an STM32 MCU. Suddenly the pipeline stopped working because of:ST-LINK firmware upgrade required. Please upgrade the ST-LINK firmware using the upgrade tool.Th...
Hello to everybody,I have a problem I can't solve with an STM32 H7 board.I wrote a little app to command a solenoid valve (24V, 200 mA). It's very simple, I have two software buttons for opening and closing it, using a relay module.Testing it, everyt...
I am trying to carry out a project with a NUCLEO-STM32G431 board.With STM32CubeProgrammer I can program the MCU without problem.But with STLM32CubeIDE I cannot program the flash.STM32CubeIDE 1.8 freshly installed (as I could not achieve anything I r...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.