Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi, I recently updated:CubeMX (6.5.0)CubeIDE (1.9.0)CubeProgrammer (2.10.0)I am having trouble with the Programmer not connecting to the targets either the Nucleo F411RE or the H7B3Li-DK. I have not tries any other types of boards.Pushing the refresh...
Hi,I designing a new design with STM32L471ZGJ6 MCU.I connected crystal osc S.N. ECS-.327-12.5-1210B-N-TR to PC14, PC15 pins in MCU.Is the value of the capacitors I connected correct? (see image below)Is the connection correct? Thanks,Mor
Hey guys,I try to connect a NUCLEO-F429ZI board with STM32CubeIDE.I have first installed the latest version of the IDE on an Windows 10 machine with the ST-LINK USB drivers that are required. When I know try to run or debug a simple example project t...
HI,I use the G0 serials firstly. I have welded 8 model machines,but I found some similar problems. For exampleOn the NO1 board, I used the pin PF1 be output.The problem is that the voltage of the MCU's reset pin is not High toVDD。So the mcu keeps r...
I'm making my ESC products in batches, after I downloaded the program for the chip, I tested the finished product and found that a lot of chips didn't work, so I downloaded the program again for the chip, but the download failed, I checked the voltag...
Hi!I download firmware to internal flash STM32H725 over STLink V2 with STM32Cube Programmer 2.9.0. Very often after downloading firmware to chip, Cube Programmer report to log window "File download complete", but firmware is not updated or chip even ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.