2022-03-10 12:56 PM
The revision history of the manual says that the schematic was removed in late 2021. Where I can download the "removed" documentation file? What was the purpose of removal?
2022-03-10 1:08 PM
<G>
Yeah, I know, less than helpful.
For some reason they decided for fork them, perhaps because a lot of manuals covered several board variants, and it became unmanageable.
The schematics are now under the "CAD Resources" tabs on the product pages rather than with the manuals in "Documentation"
Also it's basically a clone of the STM32H745I-DISCO, but that uses SMPS, the H750-DK uses the LDO, so watch that if porting code back-n-forth between those boards.
2022-03-10 1:09 PM
https://www.st.com/resource/en/schematic_pack/mb1381-h750xb-b02_schematic.pdf
2022-03-10 1:22 PM
Thanks for instant help. I was wondering about TAP-Connect and CN5 functionality... Besides, the connector CN16 was listed as "Power" in the manual but it does not feed anything.
2022-03-10 1:49 PM
CN15 is suppose to allow for a "charger" type connection, ie RPi power wall-wart, that you can jumper power from JP8 without involving the ST-LINK
Older boards the ST-LINK would often clamp target device in reset absent a PC data connection, an issues that comes and goes with firmware updates
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.