2022-03-08 11:02 AM
Hello,
We have CI/CD pipeline running in a build server with an ST-LINK attached to program an STM32 MCU. Suddenly the pipeline stopped working because of:
ST-LINK firmware upgrade required. Please upgrade the ST-LINK firmware using the upgrade tool.
The whole pipeline is automatically ran with command line tools. I would like to know how is it possible that it suddenly stopped working and how can it know that the ST-LINK firmware is outdated? This is disturbing since we are trying to keep the whole test setup as static as possible and only do controlled updates.
2022-03-08 12:28 PM
You don't mention a tool chain.
IAR/Keil might hold ST-LINK related DLLs which update, and then have expectations.
If you introduce a new board/ST-LINK, it may also be behind the version expectations of the drivers/dlls
2022-03-09 2:20 PM
We are using STM32CubeProgrammer CLI and the ST Link GDB server in Linux inside a Docker container so the environment has always been identical and nothing has changed. I am really baffled how this situation happened.
2022-03-09 3:32 PM
The only thing I can think of would be time-bombs, but I can't say I've encountered any date related triggers myself, or from forum reports.
Perhaps the ST-LINK was caught in some odd state, and the version got misreported, or defaulted to some other number.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.