Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I'm talking to a camera device on I2C1. That is working fine. I read back the data via DMA on a scan signal. This also works fine except for one bit, D6, mapped to GPIO PA6. If the output pin from the camera is connected to PA6, I2C1 stops working. F...
Seems there is an error in the STLink firmware (upgraded to the latest version just now), clock is off about 1%.
I chose STM32F030F4 as MCU for my device. I have gone through its schematic (attached for reference). I have little doubt about it. The capacitor values are written 104, that's it. Please help me find its unit, I will be too much helpful.Secondly, I ...
Messrs ST,my customer has asked to me to replace their actual microcontroller with STM32H7A3NG: the more difficult thing is the placement of decoupling capacitors because their placement is not permitted on the bottom of the PCB (as best practice for...
I developed a stm32 project for the Nucle-H745ZIQ board with stm32cube ide, there's no issue downloading the code from IDE using its debugger. However, when I tried to download with stm32cube programmer, the code doesn't run (no expected actions can ...
Please, can I install the ST-LINK, ST-LINK/V2, ST-LINK/V2-1, STLINK-V3 USB driver dpinst_amd64.exe signed for windows 10 on INTEL i5 hardware platform and Windows 11 SO?Thanks in advanceAngelo Sorbo
hi, I'm preparing the production tools for STM32F4 using ST-LINK V2 + ST-LINK_CLI.exe. Unfortunately after setting option byte (ST-LINK_CLI.exe -OB RDP=1) the power off-on cycle is required to start cpu. Is there a way to do POR using ST-LINK V2 + ST...
Hello,I was wondering if anyone has used the STM32 Virtual COM Port (VCP) on the Nucleo-144 board (MB1361) with USART or LPUART for printf debugging. As far as I can understand, PG7 and PG8 are connected to VCP through ST-Link. In this case, the outp...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.