Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Are there daughter boards available for eval board to buy?According to user manual um2198, Two 40-pin male headers CN11 and CN12 are used to connect with memory daughterboard.Two 60-pin male headers CN6 and CN7 can be used to connect a daughterboard ...
Anyone know the whereabouts of a new or used STLINK V3SET programmer tool in North America?None of the usual disty suspects have any. All are backordered.No wisecracks, please, about why one needs a programmer/debugger when you can't buy any parts t...
Anyone know the whereabouts of a new or used STLINK V3SET programmer tool in North America?None of the usual distribution suspects have any. All are backordered on this item. Even Asian distributors are out.
Hello,I'd like to erase and load an hex file on a STM32 without use the STM32CubeProgrammer as interface. Is it possible integrate the ST-LINK v2 (SWD interface) functionality in a python/C# script to automatize the erase/flashing and integrate it w...
After this second trial, the only way that I'm able to program the MCU is using the JLINK, but I would really need the STLINK-V3MINI working as expect.
I am using STM32CubeIDE V 1.9.0, with an Nucleo board with STM32F401, and STLink integrated. Debugger just stopped working. I have spent hours trying to change debugging configurations, upgrading STLink firmware, but nothing. When I press Debug I see...
Hello,I intend to use this Discovery kit together with a side board of my own.This side board needs to be powered by the Discovery board (to avoid ground problems) and could draw more than 100mA which, if I'm correct, is the current limit through the...
HelloIn my application, I use the DAC of the Micro to charge a capacitor(47uF). When the micro is power off, the voltage on the capacitor start to discharge with a high impedance resistor(6.8Megohm). I want the leakage current of the Micro I/O small ...
Hello,I use an STM32F767 microprocessor on a custom PCB and test it with power off and on conditions. After uploading the codes, I powered off and on the system. Then, the system works only while the ST link adapter is connected. Do you have any sugg...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.