STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Store Codes in the Flash Memory in the STM32

Hello,I am using stm32f767 as a microprocessor. After power off, the codes are deleted from the microprocessor. But when I checked with the STlink Utility, I saw that the codes are stored in the Flash memory. Is the reason of non operative processor ...

AE104 by Senior
  • 8689 Views
  • 15 replies
  • 0 kudos

Resolved! STM32L496G-Discovery Unknown Device

Posted on September 26, 2017 at 22:21My STM32L496G-Discovery shows up as an 'Unknown Device' in the Windows 7 Device manager.I tried connecting to it with the ST-LINK Utility, it gives a 'No ST_LINK detected' error message.Is there a way to directly...

Flash MCU SW via SWD without ST-Link

I am currently working on a HIL Setup. I want to flash my Target Software on a STM F3 via SWD. Only the SWD Pins pins are free, all other Pins are already used and can't be used for flashing the device. I have a STM H7 on the simulator of the HIL. I ...

thechris by Associate
  • 2749 Views
  • 3 replies
  • 0 kudos

Resolved! STM32L4 external SMPS

Hi guys,I'm working in a project with a STM32L412RBT6. Due to a misunderstanding, the company i'm working with, bought a big stock of STM32L412RBT6P. I just discovered the meaning of that final "P" in the code and i'm trying to figure out how big the...

STM32G0B1KET not "booting"

Hello, I designed and assembled a simple circuit around the STM32G0B1KET and after connecting my ST-link it does not seem to "boot". My circuit looks like this: Additionally, there is a red LED through a 330Ohm resistor connected to 3.3vI am poweri...

0693W00000Lx6SIQAZ.png 0693W00000Lx6TLQAZ.png

Resolved! 3.3V external power supply

Hi everyone, I need to power my F401RE with a 3.3V external power source. I read in the datasheet I need to connect the power source to the CN7 pin 12 or CN7 pin 16. Where do I connect GND signal apart from 3.3V signal?Also, from what I understood, I...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.