Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I'm learning how to make a PCB with an STM32H725IGK6 MCU (UFBGA), which will be used as a flight controller for a drone. This is the first proper attempt I've done at creating a schematic, so I would appreciate it if someone more experienced would be...
I don't know what to do, sometimes when it installed and i tried to open it, it's show's that some files are missing?
IS STM32H750 TFBGA240 PIN TO PIN Compatible to replace with STM32H755 TFBGA240
https://www.st.com/resource/en/user_manual/um2488-discovery-kits-with-stm32h745xi-and-stm32h750xb-mcus-stmicroelectronics.pdfIn the pin list fails to identify the QSPI NCS pin candidates, I had to review schematicPG6 QSPI_BK1_NCS, PC11 QSPI_BK2_NCS /...
I am an Orcad user, and there is a MB1397B Altium schematic design file with the board documents, for an Orcad user, is it possible to provide an ASCII format of Altium. :astonished_face: David Sun
While I was working to upload firmware to a board STM32CubeIDE refused to upload code until i had updated ST Link from V2.J25.S7 to V2.J39.S7, while I wanted to comply I am getting the following error. Any help is appreciated.
HI EveryoneI have ST-LINK/V2 . its working with STM32 ST-LINK Utility V4.6.0But whenever I using ST-LINK/V2 with STM32Cube Programmer V 2.8.0. ST-LINK/V2 not detect and not able to download program Even STM32cube Programmer can't recognized either ...
Hi. Currently I am trying to learn both STM32's and electronic circuits. Currently I am designing a STM32F446 LQFP64 flight computer. And I couldn't make sure that I connected the power supply correctly. And I don't know which passive components I sh...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.