STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to power NUCLEO-F303K8 or NUCLEO-L432KC with an external supply voltage of +5V?

Hi ST community!My name is Vincenzo I would like to supply my NUCLEO-F303K8 with an external supply Voltage of +5V. I prepared a Test Project which control the LED3 to blink with a certain frequency. When I supply the NUCLEO through the VIN pin or th...

0693W00000HnqdvQAB.png
VNava.1 by Associate III
  • 14758 Views
  • 5 replies
  • 1 kudos

Control GPIO of STLINK-V3SET?

The product page for  STLINK-V3SET lists the following:Multi-path bridge USB to SPI/UART/I2C/CAN/GPIOs I can see in the STM32CubeProgrammer CLI that use can use the SPI/I2C/CAN/UART functions. But can you control the state of the GPIO 0-3 pins in som...

STM32F4VET6 No ST-LINK detected a problem.

Hello,I want to use the board with STM32F407VET6 processor. But when debugging, it gives a "No ST-LINK detected" error. Also, I downloaded the ST-LINK Utility and when I press the CONNECT button, I see the same error "No ST-LINK detected". It shows a...

0693W00000Nq0ujQAB.png 0693W00000Nq0ueQAB.png 0693W00000Nq0uZQAR.png 0693W00000Nq0tIQAR.png
HF.1 by Associate
  • 2828 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.