Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I am a 10yr Arduino IDE programmer and I have a cheap ST-Link V2 (Canaduino). M5Stack provides a copy of the firmware and I would like to experiment with making it a stand alone MCU that could read inputs and respond with outputs. I would like to do ...
Hey there i am using FTP-628 MCL101 Thermal printer(https://www.fcl.fujitsu.com/downloads/MICRO/fcai/thermal-printers/ftp-628mcl101_21_50.pdf ) with STM32F429iit6.Please help me with the same.
This is a question related to an old post I wrote: https://community.st.com/s/feed/0D53W000024ZvOoSAKIn which I said that I will make some hardware modications in order to achieve the technical suggestions and manufacturer instructions. First it was ...
I have never had any issues with any of the NUCLEO boards communicating via the serial port but for some reason I can't seem to get this board to send serial data, it does show up as a serial port on the Windows Device manager and everything else app...
Hello,i intend to use a STM32H725IGK6 device in my design.The system will be suplied from a single 3.3 voltage source.Apart from VDD,VBAT pins, i see this device has some VDDLDO pins, and 3 VCAP pins.How shall i power the vddldo pins? Can i tie them...
Hi, I work for a CEM in the UK and we've run into a problem when reflowing an STM32H757XIH6 BGA onto a PCBA. Under optical microscope inspection we're seeing that the center of the component is further away from the PCB surface than the corners. The ...
Hello,I apologize if this is an obvious question, but I do not want this part to be wrong and would prefer some confirmation.I am preparing a custom board and would like to program it in an identical manner to the evaluation/nucleo boards. To try and...
Hi,Any program on my stm32f439zi board does not start when I supply the voltage from the external power supply at 3.3V, unless I connect the programmator via USB cable to the computer as well. When I disconnect the USB cable the program continues its...
Hi, This is Soyoung.ST-LINK/V2 - Can you confirm this activation product??The case was white, but it is yellowish as shown in the picture.Please let me know if the case changed.I wait for your reply.Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.