Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi All,I'm using RCC both the crystals on PC14- 15 and PH0-1 and I want to use JTEG TRACE with 4 bit synchronization but when ever JTEG TRACE enable RCC showing warning "status: Parity disbale conflict with debug jteg 4 pin"Kindly let me know what t...
Greetings !I am very new to Controllers , I need to enable and ping the Ethernet on STM32F756G-Eval Board .Can anyone kindly suggest me with the steps/procedure to enable Ethernet in STM CubeIDE so that I can ping from my PC.Thanks
Greetings for the day,I'm working on STM32H745I Discovery board for 4.3 inch Touch Screen Controller ( GT911 i2c interface) able to control LED by touching flex button, working fine as per our requirements (for reference).We're using our customized b...
I am experimenting with the USB HS peripheral on the STM32U5A9NJ Discovery Kit, and noticed that there is a signal called VBUS_SENSE which is routed to PG1 (ADC4 IN8). I've configured ADC4 to sample from this pin, and notice that the sensed voltage i...
Hi,i made up this circuit, to protect the input of the MCU. The switches pull to GND with 0 Ohm to 22kOhm, and this is also where the ESD would come in. The output_line also goes to a MCU input, and its the one i am not sure, if its protection is eno...
https://drive.google.com/file/d/1r9MhSFT5c7hjDf6kfRWHOomkzLH9iJMF/view?usp=drivesdk Hi Everyone I made a custom board keeping stm32f429 disc1 board as a reference.When I connect the the board through usb mini it's showing USB not recognised. Below is...
Hello ST Community,I am encountering a clock configuration issue that I need assistance with.I initially began with a blank template using an internal clock, and the code ran without any problems. However, when I attempted to configure a 24MHz extern...
HelIo,I connected the anode from a diode to the operating voltage and the cathode to a pinx. I need ground to make the diode glow. How can this be implemented?
Hello community!I set up a dmamux channel, which is working perfectly in unconditional mode(direct mux). Now I want to use synchronous mode, where the EXTI0 line Interrupt is the trigger(or latch), so it initiates the DMA request transactions. I get ...
I want to install and run GRBL firmware in STM32 nucleo-F401RE board to make CNC machine where stepper motors would be driven by CNC shield.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.