Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hallo,is there something I have to check if ITM_SendChar doesn't work? I mean, I have overwritten the write function in syscalls.c and enabled in the debugger settings the swv viewer at the correct clock, enabled swv trace (the same things I did usin...
Hello,I have programmed a Nucleo-L476RG with the Blinking LED example. Until there is all fine.Now, I want to load a new program on the board. Windows Explorer and ST-Link do not detect the board and cannot load a new program on the board.I bought th...
I see this note in the user manual for the STM32U5A9J-DKIs it possible to enable 3.3V output for the GPIO on the CN9 header by removing SB56 and jumping the 3V3 pin to IOREF, or would this damage the board or not have the effect I intend?
I got this error while uploading the code and I tried using ST-link utility to erase the memory but no success. How do I troubleshoot it ? :unamused_face: Thanks in advance.
My Nucleo-G031K8 can no longer be programmed using STM32CubeProgrammer or from STM32CubeIDE. When attempting to connect using STM32CubeProgrammer I receive the following text: UR connection mode is defined with the HWrst reset mode Error: Est...
I am using a STM32H743 processor and have ST's LwIP stack running correctly. At least to the point were I can use Hercules as a client and connect to the Nucleo and send a small block of data (24 bytes) to the Nucleo. I have set breakpoints in the co...
Hi everyone,I just picked up a STM32F746G discovery board to practice on, but I can't for the life of me get the built-in STLink to show in windows. By this I mean, I'm unable to power via mini-B and LD7 just flashes red. Once I change the jumper on ...
hello ST,I'm trying to use EXTI1 interrupt for a project. But the Interrupt handler is not firing. I am using the STM32Cube IDE and CubeMX for code generation. I looked into the interrupt enable registers, Mask registers, etc and all seems fine. I am...
I am using STM32 Nucleo-H743ZI2 as a I2C transmitter and Nucleo-G0B1RE as I2C Slave Receiver in interrupt mode, now i am trying to receive Variable size of data i.e. i want to keep Slave receiver size to be Maximum and want to Stop receiving when Tra...
Hi,i am working on STM32F302R8Tx and i would like to have a 490 Hz PWM on Timer15 Channel2, attached are my configuration and my code, when i measure it , i become 491,13..Hz. what can I do to get the exact 490Hz? Any Suggestions?? thank you!!! ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.