STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Stm32f042f6 - 'funny' problem with programming

Hi! Just as a comment, did anyone had that kind of problem?uC is not found or easily losing connection while erase/program.Everything is properly designed and soldered (even programmer pins are temp. soldered to board).Every connection was checked an...

oeliks by Senior
  • 5643 Views
  • 11 replies
  • 6 kudos

NUCLEO H743, troubles with ADC and LWIP

Hello,I am currently working on a project involving transferring data acquired with an ADC through ethernet.Im am using the STM32H743 MCU.I have been building small projects using LWIP, and was able to connect to the board, ping and transmit some arr...

GLeje.2 by Associate II
  • 2331 Views
  • 4 replies
  • 0 kudos

Resolved! Custom STM32 Nucleo 64 PCB without CN2

I am in the  process of designing a custom PCB board that uses the CN4 ST-link pins to flash to the processor (rather than the standard USB Micro-B connector). Through testing with a multimeter, I have confirmed that the CN4 line is connected to the ...

IS42S32400F-6BL

Hi, I'm using STM32H750-DK as an example to build my board. And I don’t know for what purpose resistors R121 - R158 are installed. Can I directly connect these pins to ground?

Screenshot_4.png
Denys_T by Associate III
  • 1950 Views
  • 2 replies
  • 1 kudos

Stlink-v3-minie upgrade

Hi! When I connect stlink v3 minie , lounch cubeide -> stlink upgrade , it only shows "V3",  nothing more. I can't open it for upgrade.Other embedded in nucleo boards stlink v3 works and can be upgraded (nucleo G431 and H723).There is an error about ...

oeliks by Senior
  • 1855 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.