STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Nucleo-H563ZI does not power on from CN1

Hello,Just got a new Nucleo-H563ZI board and I was trying to connect it to PC through the STLINK USB-C port, in order to play with it. I've checked jumper config, and all seems right, but the only thing happening when plugging in is that LD4 RED half...

Resolved! STM32U585 VDDIO2

Hello Community, I am using the STM32U585 in a design, and I have VDD at 3.3V and VDDIO2 at 1.8V.  The 1.8V rail is supplied by a 3.3V to 1.8V voltage regulator. I connected the Enable of this voltage regulator to one of the STM32U585 I/O (this I/O i...

Lamia by Associate
  • 1762 Views
  • 1 replies
  • 1 kudos

SWV error with STM32H7

We developed our code using the NUCLEO-H743ZI2 (MB1364-H743ZI-E01) where printf over SWO worked great for debugging.  Now that we have ported our code to our custom board using the STM32H743IIK package, SWV no longer works.  It won't even launch (see...

scottro by Associate II
  • 2044 Views
  • 1 replies
  • 0 kudos

Resolved! After installing the program with ST-LINK, when I turn off the power and return it, the last program I installed does not work.

Hi. I am using stm32L010C6Tx. After installing the program with ST-LINK, when I turn off the power and return it, the last program I installed does not work. I need to reload the code. I wondered if it wasn't writing to your Flash, but it looks full ...

ZKURT.1 by Senior
  • 3264 Views
  • 6 replies
  • 0 kudos

Resolved! Compatible Displays (LCD)

Hi there, Just wondering if there are any 3.5" - 5" displays that are compatible with the Nucleo-H755ZI-Q. I require a standalone screen that is not attached to a development board. I am currently using the below screen: https://www.dfrobot.com/produ...

isaacjack by Associate II
  • 3073 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.