2022-02-07 6:35 AM
Hi. I am using stm32L010C6Tx. After installing the program with ST-LINK, when I turn off the power and return it, the last program I installed does not work. I need to reload the code. I wondered if it wasn't writing to your Flash, but it looks full in cubeprogrammer. The NRST lead is connected to GND with a 100 nF capacitor. Boot0 end is idle. Any ideas as to why it might be?
Solved! Go to Solution.
2022-02-07 9:15 AM
Boot0 end is idle ??? Connect it to GND over 1k
2022-02-07 8:30 AM
Try:
Paul
2022-02-07 9:15 AM
Boot0 end is idle ??? Connect it to GND over 1k
2022-02-07 11:22 PM
Thank you for your help. Thanks to you, the program worked. This is the solution..
2022-02-07 11:23 PM
Hello, the solution is to connect boot0 to GND with a resistor.
2022-02-07 11:27 PM
To be precise: BOOT0 must read logical 0, which can be achieved:
Regards
/Peter
2024-02-19 11:33 PM
Hi, I am having the same problem. I connected the reset to pull up with 10k and the Boot0 pin to pull down with 10k.
But this does not solve my problem.I need your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.