Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello, I want to confirm on the Nucleo-H743ZI2 board, that if the HSE bypass mode is still active (can be used) when I power the board by the 3V3_EXT? I checked the manual UM2407, and it said the Debug chip will not work when the board is powered by ...
Hi ST Team,Please suggest an camera part number which i can easily interface with the 32F746GDISCOVERY Board. Kindly share the complete details. Thanks & Regards,
I have an H745ZI-Q board. I use it only with default settings. I have connected and programmed it on three different computers for learning purposes. At some point, the board stopped connecting to the computer. In STM32CubeProgrammer, the Serial Numb...
How can I measure the sleep current of the chip on the STM32F7508-DK board?
Hi, i have build up Normal mode program For CAN on board (stm32f103c8t6) setup. It is showing that data is transmitting but when I tested on board there no DataCan you tell me what is the problem??
I am using the internal RTC and powering the board through Vin, also connected is a Li ion battery to Vbat. When disconnecting Vin supply, I am observing the following: 1. The Vbat is actually powering the entire board and draining quickly, contrary ...
I am developing an application using TIM3 with Direct-mode capture compare to measure short pulse widths of 1 to 32 microsec. I am using a Nucleo H7A3ZI-Q board for development. The clock speed is 260 MHz. The Direct capture compare on Ch1 is set the...
Hallo zusammen,Ich bin noch Anfänger auf dem ganzen hier,Ich habe folgendes Problem: Ich habe ein STM32L476RG Board und möchte nun das Nucleo-GFX01M2 Display in betrieb nehmen, ich habe alle nötigen Programme heruntergeladen(ST-Link, CubeIDE, CubePrg...
Hi, thereI'm trying to integrate the STLINK-V3MODS with my STM32H745 based project.The STM32H745 MCU is powered by an external 3V3 output regulator.The STLINK-V3MODS board has the following edge pin:Which is described in the manual as an "Input for S...
I'm trying to implement a RTC using the LSE crystal of Nucleo-h743zi board (Rev.B model). In addition, I want to backup the timestamp in case of power loss. Following the reference and user manuals, I finally have my RTC worked, using RTC backup regi...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.