Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
HelloI would like to ask for some advice regarding a liquid crystal module that I would like to use with my ST Nucleo-F410RB prototyping board. The display type is BC1202A. It can display 12 characters in two lines and it has an 8-bit (or 4-bit) bidi...
Hello, Is the STM32L4P5G-DK Discovery Kit also compatible with other STM32L4P5xx components, not just the STM32L4P5AG? Thanks in advance,Sarvesh
Hi, I'm trying to get addressable diodes (WS2812, ...) working with PWM, TIM4, DMA on the NUCLEO-G0B1RE, but oh well. Something is wrong.There is nothing on the output!I tried:PWM, TIM2_CH1, DMA = code works without errors, WS2812b worksPWM, TIM3_CH1...
I have a brand new, out-of-the-box (i.e. I've not moved any of the jumpers) STM32H573I Dev Kit, When I plug in a USB-C cable into the CN10 port. Windows 10 informs me that the "USB device is not recognised".I've tried installing the ST-Link USB Drive...
Hello to all, I'm trying to debug my multi core application. I'm following the AN5286 indication but I'm in stall soon, at "Shareble ST-Link"!I'm using Keil ver 5.31 and the ST-LINK is with firmware ver V3J5M2. The problem appear with one project sel...
Hi, I am a newbie in using openocd and STM32 MCUs, I am trying to connect iwith STM32F429ZI board from my PC using Openocd via C232H FTDI cable using its JTAG interface.I am encountering JTAG scan chain error, while running openocd -f openocd.cfgI ha...
Hi,I am not a pro user of using stm32 microcontrollers and i need to know if it is possible to connect an electret microphone with a stm32 nucleo h743zi board and see any information i receive with this component.For example, i want to connect the co...
Hello,I am using the NUCLEO-G071RB and the X-NUCLEO-DRP1M1 with the X-CUBE TXPP Software Bundle.I created my project via the instructions from https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Dual_Role.Everyth...
How get lowest sleep current in STM32F7508-DK?How can I get these current values using RTC?
I am working with standby mode on the STM32F7508-DK board and measuring the standby current as 900mA. The tools I use in the program consist of LED and RTC for wake-up. What should I do to reduce this current?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.