Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Dear ST Support Team,I recently purchased the STM32H7S7-DK development board (MB1736D) and I am encountering an issue when attempting to debug my main application code. The error message displayed is:“Failed to initialize external memory!”“Error in i...
Hi, i just started with STM32G031J6 using STM32G0316-DISCO board. Using CubeIDE i have configured my second LED LD1 on pin PA11After generated the code by IDE, I added sections for flashing these LEDs. LD2 works perfectly, but there is a problem wit...
Hello,I bought STLINKV2 + small board with STM32F103C8T6. I tried to create a simple program - LED blinking - according to example in here: https://deepbluembedded.com/stm32-gpio-write-pin-digital-output-lab/ and I have STMCubeIDE + MX + others.My...
Hi, I hope Everything is fine. I have a board that uses stm32f030 as the processor. When I open an empty project on stm32, debug or run it, I get the "failed to erase memory" error. I deleted the obtion byte from cubeprogrammer and changed the st lin...
Hi team, I was trying to establish CAN communication between Matlab Simulink and 2 nodes, through STM32 board. Our logic is working fine when checked individual device. But communication is not taking place when respective nodes are connected to Can1...
I'm just looking for some clarification on a few points, having watched one or two of the training videos. I have bought a NUCLEO-G031K8 dev board, but was wondering if I could just go straight to my target board 1. in the project setup, it asks wha...
I am using NUCLEO-U575ZI-Q eval board. I am trying to blink RGB LEDs. But RED LED which is connected GPIOG pin 2 is not toggling.
I am running a 16" M2 Pro MacBook with Sonoma 14.4.1. I am able to connect to the target and start the program + debug sequence, but when the debugger attempts to erase the memory, it halts (solid green light) and throws errors:failed to erase memory...
Hello I have questions about Nucleo-F446ZE. So basically my company already has Simulink and Matlab for new members to learn MBD, and my company also has Nuleo-F446ZE. Previously, I tried to inject the program from Simulink to the Arduino device to m...
For more than 3 days I am trying to solve a problem of connecting to Riverdi board using external ST-link from a discovery board. I flashed apps without problem and now I can't do anything. I remember last time I was flashing an app it asked that fir...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.