2025-01-27 7:56 PM - last edited on 2025-01-28 7:48 AM by Andrew Neil
Hi team,
I was trying to establish CAN communication between Matlab Simulink and 2 nodes, through STM32 board. Our logic is working fine when checked individual device. But communication is not taking place when respective nodes are connected to Can1 and Can2 and checked parallelly.
Thank you,
M Satya Prashanth
9515992585
Solved! Go to Solution.
2025-01-28 7:41 AM
Hello @msp171197 and welcome to the community,
First Matlab/Simulink is not the environement developped by ST but it is developed and supported by Mathworks.
So I invite you to submit your request in their community.
Second, I can answer your first question: yes you can use CAN1 and CAN2 simultaneously in both boards:
Nucleo-F446RE and NUCLEO-F446ZE.But you need to add a CAN transceiver for each CAN instance and establish a complete CAN bus as shown in this figure.
Hope that answers your question.
2025-01-28 7:41 AM
Hello @msp171197 and welcome to the community,
First Matlab/Simulink is not the environement developped by ST but it is developed and supported by Mathworks.
So I invite you to submit your request in their community.
Second, I can answer your first question: yes you can use CAN1 and CAN2 simultaneously in both boards:
Nucleo-F446RE and NUCLEO-F446ZE.But you need to add a CAN transceiver for each CAN instance and establish a complete CAN bus as shown in this figure.
Hope that answers your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.