STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Powering NUCLEO-L412KB from +5 V

STM32L412KBUx on NUCLEO-L412KB, STM32CubeIDE, Version: 1.8.0.I'm trying to power my NUCLEO-L412KB from an external +5 V power source. I have removed SB9 (connected NRST signal of ST-LINK to the NRST pin of theSTM32). SB1 (USB power through CN1) is OF...

CKugl.1 by Senior II
  • 3373 Views
  • 7 replies
  • 0 kudos

ADC module issues in STM32F429

I am trying to capture an ADC conversion value for ADC1 channel 1 using the PA1 pin as per the STM32F429 Datasheet and have come across a couple of issues. My question has two parts, one for the actual conversion and one around the captured value.Que...

Commands LORA: P-NUCLEO-LRWAN2

Hi,  I recently bought a P-NUCLEO-LRWAN-2, and I would like to communicate through LORA from the gateway to the end-node and vice-versa, but some information is lacking. In the Getting started with the P-NUCLEO-LRWAN2 and P-NUCLEO-LRWAN3​ starter pac...

ST-LINK: Could not verify ST device

When "ST-LINK: Could not verify ST device!" error appears and what the mentioned verification process consists of? Can I influence verification process in STM32CubeIDE and how?I have STM32 MCU, which gives me "ST-LINK: Could not verify ST device!" in...

MSZ1 by Associate II
  • 8050 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.