Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi All,Thanks for advance!Actually i have selected STM32L475RET6TR MCU for my one of my project. I am looking for the best Evaluation/ development board for the above microcontroller part..i found B-L475E-IOT01A this discovery kit board...My query,...
Hi I was trying to store the status of certain pins on flash memory so that I can read from flash and resume after power cycle, I have successfully written data in flash memory, I chose the last page starting address to store my data. void write_arra...
Using he STLINKV3MOD, I2C, UARTs, GPIO and using ti for SWD are all working fine without without errors for over a month and quite intensive useThe CAN code follows the same settings in the example code:InitCAN is successful.WriteMsgCAN(&canTxMsg, ...
Hello,I need support with the following issue I am facing.I am using the discovery board STM32F407G-DISC1. When I launch the debug mode, in the SFRs window I get the error "Error reading value".I am following a course in Udemy for embedded programmin...
im looking in the bsp folder for the stm32f429i-disc in the stm32cube_fw_f4 folder and i see a file stm32f429i-discovery_eeprom.c why is this here as i dont believe there is a eeprom on this board
Hi all,I would like to keep RTC value (and keep the RTC working) during power off of the disco board, so I am planning to cut SB16 (soft bridge) from+3.3V and solder an external CR2032 +V battery to the board. My first questions are:How will I know t...
Does anyone have info or know how to determine the part #'s or specifications for lcd's used on STM32F746G-DISCO and STM324291-Eval1 boards?
Hello,Maybe you can help me, I am not able to start debug session with STLINK-V3MINIE.Context is: Windows 10 64bit, Intel(R) Core(TM) i5-9400STMCubeIDE V1.17.0 Tried with 2 different STLINK-V3MINIEthe STLINK-V3MINIE is seen and updated correctly to V...
Hi all,I am using the Nucleo-H723ZG board and I'm testing the consumption in stop mode, running the example from the ST repository NUCLEO-H723ZG\Example_LL\PWR\PWR_EnterStopMode.The code compiles without any warning and I use the stlink of the nucleo...
I have two NUCLEO-H755ZI-Q boards and I’m trying to run the SPI_FullDuplex_ComIT example on both.One board breaks here (whether the software is built for master or slave):The other board has no problem (whether the software is built for master or sla...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.