STP45N60DM2AG TO247-LL heatsink is anode or cathode or insulated ??
Hi STteam, I have selected STP45N60DM2AG MOSFET which is TO247-LL package heatsink base is anode or cathode or insulated may i know ?? it is not mentioned in the datasheet.
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hi STteam, I have selected STP45N60DM2AG MOSFET which is TO247-LL package heatsink base is anode or cathode or insulated may i know ?? it is not mentioned in the datasheet.
Is there any tolerance spec available for I_PU (the 20uA pull-up current on the outputs) of the IPS4260L?
I have the following situation:I have a custom PCB with a 4 port HUB ic on it (TUSB8041IRGCR). The UFP of the hub is connected to my phone and there are 4 DFP.My phone negotiates with the PD controller via CC lines about what voltage it wants when p...
Hi allMy team are using STC3100 for our project. But just I confusing as following itPlease see as following URTSTC3100 data sheet mentioned Rev1.1 and Date of 19 Sep 2016https://www.st.com/ja/power-management/stc3100.html#documentationBut this DL ...
Hi,I'm configuring a L9907 Driver IC using a STM32 controller. The controller is sending 0xEAAA to the driver IC, however the driver IC is not responding to the input. The MISO pin is flat at 0.Kindly help me resolve this issue
Hello, is there any way to adjust the rise and fall time of the coil driver on the STWBC86? The observed rise and fall times are currently 3-4ns, but I am looking for ways to extend them to 70ns+ due to excessive emissions with my product.Thank you!
I just bought 10 pcs of LDL1117S33R which i plan to use them to power 3.3V modules form a 4V regulated source.According to the data sheet the typical dropout is 350mV and max is 600mV @1.2A. My module consumes less than 500mA, so i expect to have eno...
Hello St community, I am designing a 24 Volt 10 amp power supply. Could you please review this design. @STM Community https://eds.st.com/acdc-qr/?msg=%7B%22data%22%3A%7B%22application%22%3A%22acdc_qr_html%22%2C%22specs%22%3A%7B%22ic%22%3A%22l6566b%...
(Split from: https://community.st.com/t5/power-management/induction-cooktop/m-p/731743) Hi everyone,I am wondering if anybody can help on an improper use of the induction cooktop .I've received an ST email featuring the STEVAL-KITXCB and it is very i...
Hi,the maximum I2C input low voltage is stated as 0,35V for the STUSB4761.Is this a typo?Because in NXP I2C spec this level is stated as 0,3VDD We are using a PCA9516 I2C Multiplexer (0,5V Low) and observe massive connection failures with STUSB4761. ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.