Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Induction Cooktop

Hi I'm looking for application note and design sources for STEVAL-KITXCB -Induction cooker Please share if anyone have this . Thanks

Resolved! Start up L6981(C33) problems

I'm using the L6981C33DR bug converter to convert 24V (from an SDR-120-24 power supply) down to 3.3V. However, I've had instances where the regulator overheats and "exploaded".The circuit only needs to supply around 100mA at startup, so the current d...

Chris_SA_0-1731060300492.png Chris_SA_1-1731060609394.png
Chris_SA by Associate II
  • 2604 Views
  • 7 replies
  • 1 kudos

Issue with STUSB1700 Negotiating BMS with SYNC

Hello,I am currently integrating the STUSB1700 into a custom circuit board design. However, I am facing an issue where the STUSB1700 is unable to negotiate the Battery Management System (BMS) with the SYNC protocol.To provide more context:The Saleae ...

VNF9Q20F and VNF1048FTR: How to get I2t Curve

Hello,I am working with these two IC's to try and create an SPI programable power distribution module. For the VNF9Q20F I understand that you set Inom and Tnom to get your desired curve. My question is how do you know what Tnom you would need to sele...

Bogdan14 by Associate
  • 866 Views
  • 0 replies
  • 1 kudos

SCT1000N170AG_V2 SPICE model uses help

Dear Engineer: Is there an error in the SPI model of SCT1000N170AG_V2? Why do I have such a simple switching circuit, and when SCT1000N170AG_V2 is turned on, the waveform is like this? Theoretically, the conduction should be 500V, and the output shou...

JAYCE_0-1732366799730.png
JAYCE by Associate
  • 746 Views
  • 0 replies
  • 0 kudos

How to set up the SPI communication with powerSTEP01

Hi beloved friends of software architecture,i try to programm an SPI communication protocol of an STM32F373CCT6. It should communicate to the powerSTEP01 in order to move a motor. The problem is that i dont get any answer of the powerSTEP01. Did i d...

SJank.3 by Associate III
  • 3559 Views
  • 5 replies
  • 1 kudos

Resolved! EVSPIN32G4 ST evaluation Board

  Hello, we're using the EVSPIN32G4 ST evaluation board. in this evaluation Board design with two microcontrollers (stm32f103cbt6 for debugging and STSPIN32G4 for motor control). Unfortunately, the STM32f103cbt6 microcontroller has failed!! We bought...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.