2024-12-01 4:26 AM
Hi STteam,
I have selected STP45N60DM2AG MOSFET which is TO247-LL package heatsink base is anode or cathode or insulated may i know ??
it is not mentioned in the datasheet.
2024-12-01 5:57 AM
This is the package variant TO-220, where tab is always connected to the centre pin, in this case drain.
Hope that helps?
Regards
/Peter
2024-12-01 8:43 AM
Sorry for mentioning wrong part number previosuly ,
i am using STPS61170CWLY diode , TO247-LL package heatsink base is anode or cathode or insulated may i know ??
2024-12-01 11:32 PM
The same statement as before applies to this double Schottky STPS61170CWLY : the centre pin is connected to the tab, because this is the result of the lead frame geometry. However, you can also check this again by carrying out a continuity measurement between the centre pin and the tab. If there is no mention of insulation in the data sheet, then there is no insulation inside the device.
I am sorry that this is not explicitly mentioned again in the data sheet.
Good luck!
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.