Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VNF1048 eFUSE Short to Battery and Open Load detection

Hi,  I am analyzing the different diagnostics capabilities of VNF1048 eFUSE.Could anyone share some details on how the Short to Battery and Open Load detection can be done for VNF1048 eFUSE output.Is there any external circuit required to detect the ...

Biju_P by Associate
  • 768 Views
  • 0 replies
  • 0 kudos

STTH110,diode failure in two-tube forward application

Hi all,   STTH110,the role of the diode in the two-tube forward circuit is the demagnetization of the transformer, which is found to burst in use.   The diode is exploded in the middle, pictured below:    The question is how did the diode break? The ...

Lihuigao_0-1733705385331.png
Lihuigao by Associate
  • 826 Views
  • 0 replies
  • 0 kudos

Resolved! L6981C50DR power module pcb design

Hi all,I selected the L6981C50DR for my DC DC buck converter with the following external components and schematic for my application:Cin: GRT31CR61H106KE01L Multilayer Ceramic Capacitors MLCC - SMD/SMT 10 uF 50 VDC 10% 1206 X5R AEC-Q200 RoHS Complian...

schematic.PNG battery_data_sheet.PNG
aferjani by Associate II
  • 2420 Views
  • 5 replies
  • 3 kudos

L6924UTR: abnormal behavior of ST1 and ST2 outputs

Hi all,   I have a problem with the L6924 in the below schematic. After ca. 1 minute of USB power both red and green LED lit and the output keeps on bouncing from 0 to 4.6V with or without battery attached. The 5V USB are stable and so is the charger...

stop by Associate II
  • 1070 Views
  • 0 replies
  • 0 kudos

Question for SPSA068 program

Application: BMSEAU: 100KSOP: 2025Q3End customer: NDA needI want to know SPSA068 if we can program by customer?How to program? Any tools we can use?Do ST can provide burning file from factory configuration?

RandyHou by Associate
  • 928 Views
  • 1 replies
  • 0 kudos

STUSB4761 rejects PDO with 5A

We try to use STUSB4761 for a 100W USB-PD Source.Test setup includes our PCB with STUSB4761 as power source, an e-marked 5A rated cable and Acroname "USBHub3c Pro Edition" as power sink.According to the log (see Attachement) of the USB PD communicati...

STUSB4761_Config_20241119_1.png STUSB4761_Config_20241119_2.png STUSB4761_Config_20241119_3.png STUSB4761_Config_20241119_4.png
mrs by Associate II
  • 10184 Views
  • 11 replies
  • 0 kudos

USBLC6-4SC6 Schematic Design Verification

Hi,We are using USBLC6-4SC6 TVS Diode in our design for USB line. The schematic is shown below:We have connected IO1 pin in parallel to D+ line and IO2 pin in parallel to D- line of USB data lines where as IO3 and IO4 lines are left open. Can you ple...

Aakash_Dey_0-1733315872271.png

Information request for L6566B Vref voltage reference.

A 24 VDC, 10 A AC/DC converter design has been done using the eDesignSuite on the ST website.     In this design, L6566B controller has been used. After production of the prototype converter, we tested the converter using loads 4-5 amps. There was no...

EDokm by Associate III
  • 1618 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.