2015-12-09 1:21 AM
Hello,
on STM8S003F3U according to datasheet there is 1024(total ram) - 513(stack) = 510 bytes for user application: 256 byte in the zero page and (510-256)= 254 in Ram section.If use the short stack compilation option all data are automaticaly maped in the zero page space and i have an error if i use more than 256 bytes.if i use the long stack compilation data are mapped automaticaly in the upper page: the Ram page and i have an error if use more than 254 (normal because there is the end stack overlap)I did'nt find any cosmic compiler user guide for stm8. If i try to use pragma to force linker to set data in different space the error is : pragma misplaced ...How is it possible to use mixed data mapping zero page and ram page ???thank's a lotregarsjohan2015-12-09 9:31 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.