Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8S TIM2 Interrupt not working

Hi, I'm trying to Implement an interrupt every 60 seconds, however something is missing. The TIM2 itself is working but can't seem to generate any interrupt. Any idea on what am i missing? The following is the code I am using. thanks //Required Hea...

SAlam.1 by Associate
  • 2777 Views
  • 3 replies
  • 0 kudos

Switch relay synchronously in 0 passage (50Hz)

i am trying to switch a relay via the stm8s001 processor synchronously in the 0 pass. how could I realize that.i have an imput signal of 50 Hz. I can also start the timer, but I don't know how to switch the relay on exactly in the 0 cycle.(i watch th...

ATürk.11 by Associate II
  • 1291 Views
  • 1 replies
  • 0 kudos

I want to reduce the power consumed by SD card

Hi,We have designed an audio system where I have interfaced MEMs microphone and freq is 32KHz and I am storing files in the SD card. The files we record are getting stored in it in real-time so sd card is continuously in use.So, we have tested that i...

SJone.2 by Associate
  • 871 Views
  • 0 replies
  • 0 kudos

Resolved! STM8AF Bootloader CAN write memory.

I'm trying to write a program to the microcontroller through the bootloader via the СAN interface.First I pass message ID 0x7f to activate bootloader. (ID=0x02, data=0x79)Then I transfer the file "E_W_ROUTINEs_128K_ver_2.0.s19" in binary form to addr...

MR.9 by Associate
  • 1795 Views
  • 1 replies
  • 0 kudos

How to generate PWM with offset / delay?

I need to generate two signals as shown below.I need to be able to adjust A and B independently. Is there some way to use TIMER1's OC1 and OC2? I can't figure out how to make an offset in the output compares - everything seems to start at the main co...

0693W00000Dq2rmQAB.png
EAnde.3 by Associate II
  • 3384 Views
  • 4 replies
  • 0 kudos

Question about "15 kW, three-phase Vienna rectifier with low cost mixed-signal control for power factor correction"

https://www.st.com/en/evaluation-tools/stdes-viennarect.htmlI have some questions about the PDF "stdes-vienna rect" that can be obtained from "Download data brief" in.1) Why is the CCO_clk on page 4 connected to DIGIN [1] and DIGIN [2]? Does it make ...

HKOBA.1 by Associate II
  • 1019 Views
  • 0 replies
  • 0 kudos

Top Marking on UFDFPN5 for M24XXX chips

What is the top marking for the following components?M24C32-FMH6TGM24C64-FMH6TGM24128-BFMH6TGThese are all UFDFPN5 packages.When marked with "4E", is that engineering samples?Is the marking "4EFT" for any of the above points?Thanks in advanced!BR,Frí...

FSigu.1 by Associate
  • 2050 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.