2016-10-24 10:56 AM
Hi
I tried to program an ST62T25C6 SO28, after loading the HEX-File in to the microcontroller with the programer (ST622X Starter kit board, release 5.00), Iput the microcontroller on to my application board and it doesn`t work. Not even the oscillator of the microcontroller works and all I/O pins are at high level.I use an adapter (dual in line 28 package to single outline 28 package) to connect the microcontrolller to the starter kit board.I can make a readout of the microcontroller content and the checksum matches to the HEX-File checksum, the options I have set, are also correct.If I program an ST62E25C DIP28 with the same HEX-File it works perfectly on my application board.The program was written in assembler language and compiled with ST6 MACRO-ASSEMBLER VERSION 4.50.I use WINDOWS EPROMER, Product ID 4.0.3,Hardware configuration ST6-004 to program the microcontrollers.I have no idea whats wrong or if I have done a mistake.I use WINDOWS 10 as OS and the Starter kit board is connected through the parallel connector to the PC.Please let me know if you need some more information.I hope you can give some ideas how to solve this issue or who I can ask otherwise.ThanksRegardsIvan #st62t25c2016-10-25 10:05 AM
Issue solved, just forgotten to add the reset vector at the end of the asm file.
But I wonder it works without reset vector on an ST62E25C.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.