2016-11-13 2:02 PM
does anyone can share bootstrap loader and monitor to proceed st10f273m CAN bootstrap?
i can successfully enter to BSL over CAN, sending frame 0 with DLC 0 and after 128 frames with id 5 and first byte of my code. It works i can execute my code but the problem is that i cant send anything from st10. Documentation says that BSL routines preparing MO 2 to be TX object with id E6 and DLC 3 and should be send for rquest by sending remote frame...BUT IST NOT!!!!!!2016-11-13 2:05 PM
and another thing, below code should make transfer MO2 via CAN....BUT ITS NOT...could abywone tell me what is wrong, please!!!
DP4 |= 0xC0; __asm{nop} P4 |= 0xC0; __asm{ DISWDT } CAN->sMsgObj[CAN_IF1].CMR = CAN_CMR_WRRD | CAN_CMR_MASK | CAN_CMR_ARB | CAN_CMR_CONTROL | CAN_CMR_DATAA | CAN_CMR_DATAB |CAN_CMR_TXRQSTNEWDAT |CAN_CMR_CLRINTPND; CAN->sMsgObj[CAN_IF1].M1R = 0xFFFF; CAN->sMsgObj[CAN_IF1].A1R = 0; CAN->sMsgObj[CAN_IF1].M2R = CAN_M2R_MDIR | 0x1FFF; CAN->sMsgObj[CAN_IF1].A2R = CAN_A2R_MSGVAL | CAN_A2R_DIR | (7<<2); CAN->sMsgObj[CAN_IF1].MCR = CAN_MCR_NEWDAT | 8; CAN->sMsgObj[CAN_IF1].DA1R = 0xADDE; CAN->sMsgObj[CAN_IF1].CRR = 2;We’re moving the ST Community to a new platform to give you a better and more reliable community experience.