Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HSO with flux weakening

I designed hardware by myself and used MCSDK 6.3.2. I chose HSO algorithm in Workbench, this work well except flux weakening feature is missing. So we cannot run motor with full load. Please advise how we can config Workbench to use HSO together with...

intania by Associate
  • 872 Views
  • 0 replies
  • 0 kudos

Resolved! STP24DP05 IC queries

Best SPI Routing Method for Double-Sided 16×128 LED Matrix Using STP24DP05Project OverviewI am designing a double-sided 16×128 RGB LED matrix display using STP24DP05 LED drivers. The LED drivers are controlled using a single SPI bus from the MCU. Sin...

clintt by Associate II
  • 2628 Views
  • 4 replies
  • 1 kudos

Issue with sx1262 module

I am trying to switch between modes (standby, rx, tx, sleep) in the sx1262 module. While switching, I pay attention to the figure below in the datasheet of the lora module. For example, to switch from SX126X_STANDBY_CFG_RC mode to RX mode, I use the ...

modes.png

Resolved! Talking to an HT16K33 via I2C

I’m connecting to an HT16K33 (on an Adafruit 4-digit, 7-segment display) to a NUCLEO-H755 board.I’m connecting I2C4 SCL to PF14 (pin 19 on CN9), and I2C4 SDA to PFf15 (pin 21 on CN9).Here's my init:static void MX_I2C4_Init(void) { hi2c4.Instance ...

SoCalJim by Associate III
  • 1776 Views
  • 2 replies
  • 0 kudos

STDV Problem

Posted on May 12, 2018 at 15:28Hi everyone. I am working with STDV development tool. When I want to build the program, the message 'the executable can not be found' appear. How can I modify the settings to solve this problem??

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.