2018-05-12 6:28 AM
2018-05-14 12:26 AM
Hello,
Which C compiler you would like to use in your project?
May I ask you to pass me a screenshot from your settings of the project, please (please click left button on mouse over the project name and select Settings, then please select General tab)?
First thing which I would check is whether the toolset paths are set correctly (compiler, linker).
Thank you in advance,
Best Regards,
Artur
2025-03-10 7:25 AM
STVP=St visual programmer, STVD=St visual Develop, NOW STDV=??? i want to debug stm8 series MCu. what software i need?
2025-03-15 5:42 AM
Use STVD. STVD already have STVP. You should start with a development board and it already have ST-Link.
2025-03-15 9:31 AM
COSMIC compiler working fine. compiled wwithout error, then build no issue, then burn by stVP help of cloned stlink-v2 usb type ,no issue programe run at MCU. but when i go to debug in STVD it says communication error 30006. have a look screen shot. if stlink cloned i am using swim pin working when programe uploading, but debuging mode not working. taken screen shot from logic analyzer, if you would like to deep dive.
2025-03-15 9:33 AM
2025-03-15 9:38 AM
2025-03-15 9:43 AM
2025-03-16 1:40 AM
You should use a development board as STM8S-DISCOVERY or use ST-LINK/V2 in-circuit debugger/programmer for STM8 and STM32.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.